Detailed Procedures - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

You need the following items to perform the detailed commissioning procedures for an SNE:

  • an SNE with Release 12.0 software

  • an Internet browser on a laptop or desktop computer to download the Launcher application that is used to log on the SNE. Supported browsers include Microsoft Edge 91 or later, Google Chrome version 91 or later, or Apple Safari version 13.1 or later

    Note: In some scenarios, the computer must be a DHCP client or must be configured to use a static IP address appropriate for the network.
  • the SNE Ethernet MAC address

You may also need:

  • a new, unique IP address for each SNE on the Metasys network if DHCP cannot be used

  • a copy of the SNE archive database that configures the SNE for your specific site. (The SNE archive database can be created and stored offline in the SCT.)

  • SCT Release 15.0 or later loaded on the commissioning computer