Setting the time zone on the Metasys Server Site Director - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

Procedure

  1. In the lower-right corner of the Metasys Server computer screen, click the time. The Date and Time Properties box appears (Figure 1). The appearance of this screen and others vary depending on the operating system.
    Figure 1. Time and Date on a Metasys Server

  2. Depending on the operating system, click Change date and time settings or Date and time settings. The Date and Time window appears, as shown in Figure 2.
    Figure 2. Date and Time window on Metasys Server

  3. Verify that the Set time automatically option is set to On.
  4. Select the correct time zone under the Time zone drop-down list box.
  5. Select Adjust for daylight saving time automatically.
  6. Close the window to save your changes.