Procedure
- Log on the Site Director network engine.
- Drag the Site object to the Display frame.
- Click Edit.
-
In the Time section, in the Default Time Zone drop-down box,
select the correct time zone for the device, as shown in Figure 1.
Figure 1. Default Time Zone in the Site Object
-
Click Save.
Note: The Site object's focus window is updated immediately to indicate the current time and selected time zone, but the blue status bar in the lower right corner does not update until you log off, then log on the network engine again.
- Reset the network engine for the time zone change to take effect.