Setting the date and time in the Site Director Network Engine - Metasys - LIT-12013352 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - Supervisory Device - SNE10 Network Engine - SNE11 Network Engine - SNE22 Network Engine - SNE Supervisory Network Engine - 12.0

SNE Commissioning Guide

Brand
Metasys
Product name
SNE10 Network Engine
SNE11 Network Engine
SNE22 Network Engine
SNE Supervisory Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active
Language
English

About this task

To set the date and time for a network engine that is configured as the Site Director, complete the following steps:

Procedure

  1. In the navigation tree, right-click the Site object and select Command. The Command dialog box appears.
  2. Click Set Time and enter a value in the text box, as shown in Figure 1.
    Figure 1. Time in Site Director Network Engine (SNE example)

  3. Click Send.
    Note: If you have a site time server selected, do not attempt to set the time manually. If you have one or more site time servers defined, sending this command generates an error.
  4. In the navigation tree, right-click the Site object and select Command. The Command dialog box appears.
  5. Click Set Date and select a date from the calendar, as shown in Figure 2.
    Figure 2. Date in Site Director Network Engine (SNE example)

  6. Click Send.
    Note: If you have one or more site time servers defined, sending this command produces an error. If you have a site time server defined, do not use this command to set the time manually.

    The Site Director time zone, date, and time are now set and propagate to all other child devices on the site. Note that it may take up to 10 min for all devices to synchronize.