Setting the date and time in the Metasys Server Site Director - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

To set the date and time for a Metasys Server that is configured as the Site Director, complete the following steps:

Procedure

  1. In the lower-right corner of the Metasys Server computer screen, click the time. The Date and Time Properties box appears, as shown in Figure 1. The appearance of this screen and the next screen vary depending on the operating system.
    Figure 1. Time and Date on a Metasys Server Site Director

  2. Depending on the operating system, click Change date and time settings or Date and time settings. The Date and Time window appears (Figure 2).
    Figure 2. Date and Time window on Metasys Server Site Director
  3. Click Change. On the Change Date and Time dialog, set the date and time.
    Note: If your operating system has the Change Set time automatically option set to On, the date and time are controlled by an external time server.
  4. Click Change to save your changes, then close the dialog box. The Site Director date and time are now set and propagate to all other child devices on the site.