Configuring Site Director for Windows time synchronization - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

To set the time synchronization method to Windows for the Site Director, either the Metasys Server or a network engine, complete the following steps:

Procedure

  1. Log on the server or network engine Site Director.
  2. Drag the Site object of the Site Director to the display frame.
  3. Select Advanced.
  4. Click Edit.
  5. In the Time section under the Time Sync Method drop-down box, select Windows.
    Figure 1. Time Sync Method field set to Windows
  6. Click Save.
  7. If you changed the Time Sync Method from Multicast to Windows, manually start the win32time service or restart the Site Director, because this service does not restart on its own.