Download certificate - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

Use the Download Certificate option to download server certificates independently from other actions. This method is much faster than if you were to download the full database with the Download To Device option under Manage Archive.

When you download certificates to a site device, SCT determines the correct set of certificates required by that device for successful site configuration. If any certificates are missing, SCT includes the set of certificates that it recognizes during the download, but the missing certificates need to be imported before trusted connections can be established. Also, no certificates are downloaded if the server certificate and private key for that device are not present in the SCT archive.