About this task
To upload a certificate from a network engine to an archive database, complete the following steps:
Procedure
- Open the archive database.
- On the Tools menu, select Certificate Management. The Certificate Management screen appears.
-
Click the Devices tab. A table of devices with
certificates appears. Select the device that has a certificate you want to
upload. (If you need to upload the certificates of multiple engines, you can
select more than one from the devices table.)
Figure 1. Uploading a Certificate
-
Click Upload. The Certificate Upload Wizard
appears.
Figure 2. Certificate Upload Wizard
- Specify the username and password of the network engine (or click Communicate via Site Director to use the Site Director's credentials). Click Test Login. When the login is confirmed, click Next to complete the remaining steps in the Certificate Upload Wizard. The ActionQ window appears to indicate the progress of the upload. A completion status of OK indicates that the certificate upload process was successful.
- Close the ActionQ window.