Importing a certificate - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

To import a certificate for a network engine in an archive database, complete the following steps:

Procedure

  1. Open the archive database.
  2. On the Tools menu, select Certificate Management. The Certificate Management screen appears.
  3. Click Import Certificates. The Import Certificates dialog box appears.
    Figure 1. Request Certificate Screen
  4. Select the certificate file. The file has a .crt, .cer, or .pem extension. Click Import. The certificate for the network engine is imported.
    Figure 2. Import Certificates Screen
  5. Click the Certificates tab to view the newly imported certificate.
    Figure 3. Newly Imported Certificate