Exporting a certificate - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

To export a certificate for a network engine in an archive database, complete the following steps:

Procedure

  1. Open the archive database.
  2. On the Tools menu, select Certificate Management. The Certificate Management screen appears.
  3. Click the Devices tab. A table of devices with certificates appears. Select the device whose certificate you want to export.
    Figure 1. Exporting a Certificate
  4. Click Export Certificate(s). The Export Certificates dialog box appears.
    Figure 2. Export Certificate(s) - Select Folder Screen

  5. Click Export Certificate(s). The certificate file is exported to the selected folder location. For example, if the name of the NAE is NAE-1, the certificate file would be called NAE-1.pem.