Downloading a certificate - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

To download a certificate to a network engine from an archive database, complete the following steps:

Procedure

  1. Open the archive database.
  2. On the Tools menu, select Certificate Management. The Certificate Management screen appears.
    Figure 1. Downloading a Certificate
  3. Select the device that has the certificate you want to download. (If you need to download the certificates of multiple engines, you can select more than one from the devices table.) Click Download. The Certificate Download Wizard appears.
    Figure 2. Certificate Download Wizard
  4. Specify the username and password of the network engine (or click Communicate via Site Director to use the Site Director's credentials). Click Test Login. When the login is confirmed, click Next to complete the remaining steps in the Certificate Download Wizard. The ActionQ window appears to indicate the progress of the download. A completion status of OK indicates that the certificate download process was successful.
  5. Close the ActionQ window.