Deleting a certificate request - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

To delete a network engine certificate request from an archive database, complete the following steps:

Procedure

  1. Open the archive database.
  2. On the Tools menu, select Certificate Management. The Certificate Management screen appears.
  3. Select the device whose certificate request you want to delete. Click Delete. A confirmation message appears.
    Figure 1. Delete CSR Confirmation Message

  4. Click OK to delete the certificate request. The certificate requests list refreshes indicating that the certificate request has been removed.