Backing up a certificate - Metasys - LIT-12013352 - M4-SNE10500-0 - M4-SNE10501-0 - M4-SNE11000-0 - M4-SNE11001-0 - M4-SNE110L0-0 - M4-SNE110L1-0 - M4-SNE22000-0 - M4-SNE22001-0 - Supervisory Device - SNE10 Network Engine - SNE11 Network Engine - SNE22 Network Engine - SNE Supervisory Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

About this task

To back up a certificate for a network engine, create a backup of the archive database using the traditional method in SCT (Tools > Database > Create Backup). In addition to backing up the archive database, this process also backs up the network engine certificates. For details, refer to the Create Backup section in Metasys SCT Help (LIT-12011964). You can also back up and store certificates for safekeeping by exporting each certificate file to a computer or removable media. Refer to the Exporting a Certificate section in Metasys SCT Help (LIT-12011964). Lastly, certificates are also backed up and stored when you export the archive database. Refer to the Export Database section in Metasys SCT Help (LIT-12011964).
Important: As an important restriction for creating and restoring database archive backups that contain network engine certificates, you must use the same SCT computer for both operations. Do not restore the archive using a different SCT computer, or the certificate data is deleted. This is a security precaution that protects against certificate theft.