Certificate list view - Metasys - LIT-12013352 - M4-SNE110L0-0 - M4-SNE10501-0 - M4-SNE22001-0 - M4-SNE10500-0 - M4-SNE11001-0 - M4-SNE110L1-0 - M4-SNE11000-0 - M4-SNE22000-0 - Supervisory Device - SNE Supervisory Network Engine - SNE22 Network Engine - SNE11 Network Engine - SNE10 Network Engine - 12.0

SNE Commissioning Guide

Product
Network Engines > Network Control Engines > SNE22 Network Engine
Network Engines > Network Control Engines > SNE11 Network Engine
Document type
Commissioning Guide
Document number
LIT-12013352
Version
12.0
Revision date
2022-12-12
Product status
Active

Use the certificate list view to determine if all certificates required by each device reside in the archive. The certificate list view provides these features:

  • Indication of an expired certificate.
  • Indication of whether a certificate is required in one or more certificate chains used by a device in the archive. The list view also makes clear which certificates are not needed and may be deleted.
  • Information about the certificate, including: Issued To, Type, Device Name (server certificates), Expiration Date, Details (for example, SHA1 Thumbprint).
  • Clickable column headers that sort the rows by the data in that column.
  • Options for importing, exporting, and deleting root, intermediate, or server certificates.
Figure 1. Viewing Certificate Details