Wizards - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Wizards make complex tasks easy and guide you through creating and configuring objects and features. A wizard typically consists of a series of steps, each corresponding to a screen presented to the user.

A wizard may appear when you select an option from the Insert menu and when you prompt certain actions such as copying and pasting an item in the Navigation Tree. For example, a wizard appears when you select Object from the Insert menu. Wizards that are available in different modes (for example, any combination of online or offline) appear the same.