Working in the SCT UI - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Objects in the SCT user interface are now easily searchable in the navigation trees through the Locate in Tree feature. The Locate in Tree feature displays the expanded Equipment, Spaces, or All Items tree location for an object selected from the focus window.

To use this search feature, right-click one of the following object name locations and select Locate in Tree:
  • Global Search table rows
  • An object's Focus window title bar
Figure 1. Locate in Tree Option
Note: Locate in Tree search feature is not compatible with User Views and the Unlicensed Item trees.