Related documentation - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English
Table 1. SCT related documentation

For Information On

See Document

SCT features, benefits, and requirements

System Configuration Tool Catalog Page (LIT-1900198)

SCT installation and upgrade

SCT Installation and Upgrade Instructions (LIT-12012067)

Licensing SCT and field controller packages

Software Manager Help (LIT-12012389)

Daily use of the Metasys system, and database backup/restore

Metasys Site Management Portal Help (LIT-1201793)

SCT interaction with the ADS/ADX

ADS/ADX Commissioning Guide (LIT-1201645)

SCT interaction with the ODS

ODS Commissioning Guide (LIT-12011944)

SCT interaction with the NAE/NIE

NAE Commissioning Guide (LIT-1201519)

SCT interaction with the NIEx9

NIEx9 Commissioning Guide (LIT-12011922)

Backing up and restoring driver and license files before updating the NIEx9 image

NIEx9 Driver Manager Application Note (LIT-12011919)

Adding users and roles to the system

Security Administrator System Technical Bulletin (LIT-1201528)

Configuring the ADS/ADX as a trusted server with https

Metasys Server Installation and Upgrade Instructions (LIT-12012162)

General network and information technology concepts

Network and IT Guidance Technical Bulletin (LIT-12011279)

Metasys configuration

Metasys System Configuration Guide (LIT-12011832)

Metasys system

Metasys System Extended Architecture Overview Technical Bulletin (LIT-1201527)