Prerequisite Software Checklist for SCT Installation - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The computer operating system that you want to use for SCT software must have the correct components installed. SCT software does not install or function correctly if any of these components is missing. The SCT Installation wizard verifies that the computer has these prerequisites, but make sure you carefully review the software requirements listed in Table 1 before you install SCT. The table also indicates where you can obtain each software component. For detailed information about installing the SCT software, refer to the SCT Installation and Upgrade Instructions (LIT-12012067).

Table 1. Prerequisite Software Checklist for SCT

Software Component

Product

Where to Obtain

Operating System (select one)

Windows® 11 Pro and Windows® 11 Enterprise Editions (version 21H2, 22H2) (64-bit)

ADS/ADX

SCT

Microsoft Corporation

Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit).

Windows® Server® 2022 (64-bit)

Windows® Server® 2019 (version 1803) (64-bit)

(Standard or Enterprise Edition)

Operating System (OS) Components (select all)

Internet Information Services (IIS) (included with OS)

ADS/ADX

SCT

OS media

Microsoft Message Queuing (MSMQ)

ADS/ADX

SCT

Miscellaneous (select all)

Daylight Savings Time (DST) Patch for OSs

ADS/ADX

SCT

http://www.microsoft.com/downloads

Microsoft .NET Framework 3.5 SP1 or 3.5.1

http://www.microsoft.com/downloads

Microsoft .NET Framework 4.7.2

ADS/ADX

SCT

SCT Media. Microsoft .NET Framework 4.7.2 is installed with the System Configuration Tool Setup if it does not already exist on the computer.

Database (select one)

SQL Server 2019 Standard, Enterprise, and Express CU6 (64-bit)

ADS/ADX

SCT

ADS/ADX or SCT media

Note: For an ADX installation use the Standard or Enterprise version of SQL Server, which you can obtain from the Microsoft Corporation.
SQL Server 2017 Standard, Enterprise, and Express CU21 (64-bit)

Database Tools (select if required)

Microsoft SQL Server Management Studio Express

ADS

SCT

ADS/ADX or SCT media

Note: A software database management tool for SQL Server Express software editions without management tools. This tool ships bundled with the Standard and Enterprise editions of SQL Server 2014 and earlier software.