- For Release 5.2 and later, the Rediscover Text Strings operation generates custom enumerations from all mapped BACnet and MS/TP objects. These custom enumerations are backed up when the Site Director is uploaded in the Release 5.2 database. During the upgrade process, a restored, upgraded, or downloaded Release 5.2 database maintains these custom enumerations during the upgrade process.
- For Release 6.5 and later, the User Defined States Text attribute is set to true whenever an object has a custom enumeration set assigned to it.
- Engines at Release 8.0 and later automatically read custom state sets text created in CCT and display them in the SMP user interface, instead of the generic State 0 to State X text.
|
Name |
Use |
|---|---|
|
Add and Delete Custom Enumeration buttons. |
Add new or Delete existing User Defined Enumeration Sets. |
|
Edit OR Save and Cancel Buttons. |
When you select the Custom Enumeration tab there is an Edit button here; upon selecting Edit, the button is replaced by the Save and Cancel buttons. |
|
Name |
Name of the new or selected Enumeration set - limited to 32 characters. |
|
Size |
Enumeration set size. This is the number of values within the selected enumeration. You may not see optimal performance if this exceeds 5 members. |
|
Enumeration Entries |
Entries within the selected enumeration. Cannot be blank or white space. You may not see optimal performance if this exceeds 10 characters. |
|
List of existing user defined enumeration sets. |
Displays the current list of User Defined Enumerations. This list is limited to 256 entries. |