The Syslog tab appears on Engine or Server objects. The Syslog DDA Attributes appear on the Shared Configuration section of the Syslog Tab. The Syslog DDA destination Configuration Attributes appear when you edit or create a new Syslog Destination on the Syslog tab.
Syslog has one Share Configuration attribute—Syslog Reporting Enabled. When the Syslog Reporting Enabled attribute is set to True the feature is active and your error logging is forwarded to your destination server.
For more information on Syslog and configuring other DDAs, see the Configuring Destination Delivery Agents (DDAs) section in Metasys SMP Help (LIT-1201793) or Facility Explorer Site Management Portal Help (LIT-12013520).
Attribute | Value / Description |
---|---|
Label | Destination name |
Syslog Server | IP Address for the destination server |
UDP Send Port | The designated port on the device for error transmitting to your server. |
UDP Receive Port | The designated port on your server for receiving the error transmits. |
Event Filters | To add or remove Events from displaying |
Audit Filters | To add or remove Audits from displaying |