VND Hardware Tab - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Attributes associated with the hardware source for object data are shown under the Hardware tab of the display panel. Attributes marked with the letter C are configurable and attributes marked with the letter W are writeable.

Table 1. VND Hardware Tab Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Disable Automatic Alarming

C,W

False

 

Field Value

   

Applies to only AI, AO, BO, MI, and MO objects.

Interface Value

   

Applies to only AI, AO, BO, MI, and MO objects.

Max Value

C,W

250.0 deg F

Applies to only AO objects.

Min Value

C,W

-50.0 deg F

Applies to only AO objects.

Offline

   

Applies to only AI, AO, BI, BO, MI and MO objects.

Overridden

   

Applies to only AI, AO, BO, MI, and MO objects.

Priority

C,W

 

Applies to only AI, AO, BO, MI, and MO objects.

Protocol Description

C

VendorDriver

 

Protocol Revision

C

   

Protocol Revision Date

C

   

Protocol Review Time

C

   

Temporary Status Item Expiration Time

C,W

 

0–65,535

Units = Seconds

Trouble

   

Applies to only BI and BO objects.

Vendor Configuration Data

C,W

 

Maximum characters = 80

Maximum entries = 128

Vendor DLL

C,W

VENDOR.DLL

 

Vendor Integration Size

   

Units = bytes

Vendor Reference

C

   

Vendor Revision Date

C

   

Vendor Revision Time

C