LonWorks Hardware Tab - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Attributes associated with the hardware source for object data are shown under the Hardware tab of the display panel. These attributes are not exposed to a BACnet network. Attributes marked with the letter C are configurable, and attributes marked with the letter W are writable.

Table 1. LonWorks Hardware Tab Attributes

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Alarm Event State

C,W

True

False

True

Specifies whether Node State changes will cause alarms. The value of True allows Node State alarms to be processed by the NxE. The value of False masks Node State alarms from the NxE.

Command Status Mapping Table

C,W

 

Applies to BI, BO, MI, and MO objects only.

Custom Scale/Offset

C,W

 

Applies to AI and AO objects only.

Device Class

   

Maximum Length = 40

Category = Default

Device Subclass

   

Maximum Length = 40

Category = Default

Disable Automatic Alarming

C,W

False

False

True

Domain ID

C

01

Maximum Length = 12

Category = Default

Hex bytes of length 0,1,3, or 6

Driver Name

 

Ipcdrv

Maximum Length = 30

Category = Default

DSN 1

C

 

Maximum Length = 30

Category = Default

DSN 2

C

 

Maximum Length = 30

Category = Default

Enable Polling

C,W

 

Applies to AO, BO, and MO objects only.

Field Units

C,W

DegF

Uses Unit Set (Set 869).

This attribute is for AI and AO objects only.

File Filter

W

 

Maximum Length = 40

Category = Default

  • eng
  • enm
  • enu
  • fmt
  • fpt
  • typ
  • xif

File Filter can be edited for alternate languages and must be in the xxx file format.

Interface Value

     

LNS Database Name

C,W

 

Maximum Length = 30

Category = Default

Location Label

   

Maximum Length = 30

Category = Default

Manual Control

   

Applies to AO, BO, and MO objects only.

Manufacturer

   

Maximum Length = 40

Category = Default

Message Retry Count

C,W

1

Range = 0–15

Model

 

0

 

Neuron ID

   

Fixed Length = 6

Category = Default

Offline

     

Overridden

     

Priority

   

1–3

Program ID

   

Number of Elements = 40

Category = Default

Resource File Language

C,W

ENU

Maximum Length = 3

Category = Default

Status Launch Interval

C,W

0

Range = 0–10,000 milliseconds

Target Reference

C

   

Temporary Status Item Expiration Time

C,W

60

Range = 0–65,535 seconds

Immediate (0), Never (65,535)

Transceiver

   

Maximum Length = 40

Category = Default

Trouble

   

Applies to BI and BO objects.

Update Interval

C,W

 

Units = Seconds

0–65,535

Applies to AO, BO, and MO objects only.

XIF Present