Focus Tab - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Focus tab appears when you define an object in the online Site Management Portal. The Focus tab shows operation attributes available for the object type to which the object belongs. The attributes displayed on the Focus tab varies by object type. For example, the Analog Input object’s Focus tab has different attributes than the server object’s Focus tab. See the specific object section for details on its Focus tab.

Note: This tab is called the Configuration tab in the SCT or in a wizard.