Configuration Tab - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The Configuration tab appears when you define an object in the SCT or in a wizard. The Configuration tab shows operation attributes available for the object type to which the object belongs. The attributes displayed on the Configuration tab vary by object type. For example, the Analog Input object’s Configuration tab has different attributes than the server object’s Configuration tab. See the specific object section for details on its Configuration tab.

Note: This tab is called the Focus tab in the online Site Management Portal.