Associated Graphic Tab - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Associated Graphic tab appears when a graphic is referenced from the object using the Graphic attribute. Refer to the User Graphics Tool section in Metasys SMP Help (LIT-1201793) for details on working with this tab within the Metasys system and the User Graphics Tool section in Facility Explorer Site Management Portal Help (LIT-12013520) within the FX system.