Object and Feature Tabs - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

This section describes the tabs of the display panel for the objects and features in the system. Each display panel can contain different tabs depending on the item being viewed, and each tab shows different information.

Note: This section contains detailed information about the tabs used by multiple objects/features. When a tab only appears for a specific object/feature, the details of that tab are defined in that object/feature section. However, this section includes a brief description of such tabs and provides links to the detailed object/feature sections.