Object Naming Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Every object can be identified by one of three naming attributes.

Name - a freely definable user name for the object

Item Reference - a fixed name used internally by the system

BACnet Object Name - the name exposed to a BACnet network based on the Item Reference, or the name based on the User Name Is BACnet Obj Name common attribute setting

See the Object and Feature Tabs section for more information on these attributes.