Enum Finder - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The Enum Finder provides users advanced searching capabilities of enum sets for objects with the States Text attribute. With the object displayed in the focus window, click the Search (magnifying glass) icon next to the States Text attribute in the Configuration Tab in Edit mode to access the Enum Finder.

Table 1. Enum Finder Dialog Box

Screen Area

Description

Search Criteria

Allows you to enter enum set search criteria.

Results

Displays the prioritized search results for cross column searching of Set ID, Set Name, Enum ID, and Enum Value based on search criteria.

Additional Search Criteria (+) icon

Adds additional Search Criteria rows.

Ok

Applies the selected enum set to the States Text attribute of the object displayed in the focus window.

Cancel

Closes the Enum Finder without applying changes.

  1. With the object displayed in the focus window, click Edit in the Configuration tab.
  2. Click the Search icon next to the States Text attribute drop-down. The Enum Finder dialog box appears.
  3. Enter enum search criteria text or numerical strings in the Search Criteria text box. The Results table auto-populates with results listed in priority order by best matches against search criteria.
    Note: For optimal searching, add more search criteria by clicking the Additional Search Criteria (+) icon.
  4. Select the enum set from the Results table and click Ok. The Enum Finder closes and the set is populated in the States Text attribute of the object displayed.
  5. Click Save.