Values/Options/Range - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Based on the attribute’s data type, this column may show the range of valid values or a reference to the set of possible values for this attribute. If the complete set of values for the attribute is small, all possible values are shown in this column.