Common Object Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The Common Object Attributes are used by most of the object types in the systems. Each object type also has specific attributes that apply only to that object type. A reference to the use of Common Object Attributes and a description of specific object attributes are given under each particular object in the Object List.