The following shows SCT as part of an overall Facility Explorer network. The SCT is installed on, and can be accessed by, a computer on the building network.
Figure 1. SCT as Part of a Facility Explorer Network
The following shows SCT as part of an overall Facility Explorer network. The SCT is installed on, and can be accessed by, a computer on the building network.