Metasys and FX system overview - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The major components of the Metasys system are:

ADS/ADX: The Application and Data Server (ADS) is a software package that you can use to monitor and control the entire Metasys system. The ADS also serves as a long-term storage device for alarm and event messages, trend data, and user transactions. For customers with large facilities, the Extended Application and Data Server (ADX) is available to provide extended user access and historical data storage capabilities. You can use an ADS/ADX to access the user interface and to serve as the location for user graphics. The ADS/ADX typically coordinates multiple user access from web browsers to the network. Hereafter, the term Metasys Server applies to either the ADS or the ADX.

You can also install the ADX in a split configuration with the ADX software/user interface on one computer (the web/application server computer) and the historical trend data on another computer (the database server computer).

OAS: The Open Application Server was introduced in Metasys Release 10.1. You can use an OAS as the point of access into a building automation system (BAS) and to archive historical and configuration data for a site. You can use an OAS as the supervisory device for 200 or fewer field devices through BACnet/IP or Remote Field Bus protocols. As a Site Director, an OAS can also support two child NxE or SNx devices. The OAS is an ideal solution to add the Metasys UI to an engine-only site. Hereafter, the term Metasys Server also applies to the OAS.

Network Engine: The network engine is a family of devices that supervise lower-level field controllers over the Metasys BAS. Network engines include the Network Automation Engines (NAEs), Network Integration Engines (NIEs), Network Control Engines (NCEs), Series of Network Controllers (SNCs), and Series of Network Engines (SNEs):

  • The NAE and SNE are Ethernet-based supervisory engines that monitor and supervise networks of field-level building automation devices that typically control HVAC equipment, lighting, security, fire, and building access. The features of NAEs and SNEs include alarm and event management, trending, archiving, energy management, scheduling, and password protection through their embedded Site Management Portal. Different models and options support various communications protocols, including BACnet® over IP, BACnet MS/TP, Johnson Controls® N2 Bus, LonWorks, Modbus®, M-Bus, and KNX. The NAE55 and SNE2200x Series support a comprehensive set of supervisory features and functions for large facilities and technically advanced buildings and complexes. The NAE35, NAE45, SNE1050x, and SNE1100x Series support the same features and functions of the NAE55 and SNE2200x engines, but are designed for smaller buildings (or small areas of larger buildings) and enable the wider distribution of supervisory functions in larger facilities. Lastly, the NAE85 supports large BACnet/IP integrations with over 10,000 objects.
  • The NCE and SNC combine the network supervisor capabilities and IP network connectivity of a network engine with the Input/Output (I/O) point connectivity and direct digital control capabilities of a field controller. The NCE and SNC are a cost-effective solution designed for central plants and large built-up air handler applications. All NCE and SNC models include IP Ethernet network connectivity, the Site Management Portal, and the network supervisory functions featured on network automation engines. Some NCE and SNC models include an onboard display with keypad. The NCE and SNC support a wide variety of building networks such as BACnet/IP, BACnet MS/TP, Johnson Controls N2 Bus, LonWorks, Modbus, M-Bus, and KNX.
  • The NIEx5 is an Ethernet-based, supervisory engine for integration of Metasys N1 Networks. The NIEx5, which includes the NIE55 and NIE85, is a specialized version of the NAE and is designed to provide for the migration of existing N1 networks into the Metasys system. The NIEx5 has the same Site Management Portal as the NAE. Unlike the NAE, the NIEx5 does not support integration of BACnet MS/TP or BACnet/IP, N2, and LonWorks networks. Two models of the NIEx5 are available. The NIE55 supports smaller N1 networks, while the NIE85 supports larger N1 integrations. The NIE55 and NIE85 engines were retired at Metasys system Release 9.0.
  • The NIEx9 is an Ethernet-based, supervisory engine for integration of building control devices that communicate over the Modbus®, MBus, or KNX protocol. The NIEx9 also communicates over the BACnet MS/TP, BACnet/IP, N2, or LonWorks networks. This specialized version of the NIE is designed to provide for the migration of these existing third-party networks into the current generation Metasys system. The NIEx9 provides the same Site Management Portal UI as the NAE or NIE. Several models are available: NIE29, NIE39, NIE49, NIE59, and NIE89. The NIE29, NIE39, and NIE49 engines were retired at Metasys system Release 9.0.7.

SCT: You can use the System Configuration Tool in all phases of engineering, installing, and commissioning of devices that make up the Metasys system. You can use the SCT offline to create archive databases that can be downloaded to an Engine or Server. You can also use the SCT to upload and archive databases that were created or edited online from an Engine or Server. With the SCT, you can view and configure multiple sites in one archive.

SCT no longer requires the Site Director to be of an equivalent release version as the tool. You can use the SCT also to maintain a variety of engines from Release 5.2 and later. The Site Director must now be at an equivalent or greater release version than the highest versioned engine. For example, if you have a 10.1 engine and an 8.0 engine in the archive, the Site Director needs to be at Release 10.1 or later.

SCT has the same look and feel as the Server Site Management Portal.

Metasys system configuration requires that you define a single device as the Site Director. The Site Director device may be a network engine or server, and its primary role is to coordinate multiple-user access from the web browser to the network. If a Metasys server exists in the system, it is defined as the Site Director automatically. When communicating directly to Metasys servers or network engines, you are in the online mode. For information on the online and offline modes of operation, see the mode section.

Note: In order to use HTTPS communications between Metasys SMP and SCT, you must have SCT Release 11.1 or later, SMP Release 8.1 or later, and the latest version of Launcher installed.

The major components of the Facility Explorer system are:

SNC:

The SNC is a family of devices that supervise field controllers. The SNC combines the network supervisor capabilities and IP network connectivity of an Supervisory Controller with the Input/Output (I/O) point connectivity and direct digital control capabilities of a field controller. The SNC is a cost-effective solution designed for central plants and large built-up air handler applications. All SNC models include IP Ethernet network connectivity and the Site Management Portal. The F4-SNC supports BACnet/IP and BACnet MS/TP communication protocol.

SCT:

You can use the System Configuration Tool in all phases of engineering, installing, and commissioning of devices that make up the Facility Explorer SNC system. You can use the SCT offline to create archive databases that can be downloaded to an F4-SNC. You can also use the SCT to upload and archive databases that were created or edited online from an F4-SNC. With the SCT, you can view and configure multiple sites in one archive.

Important: The term F4-SNC system references either a particular F4-SNC and its subordinate devices or two or more F4-SNCs networked as peers. This definition does not include the FX Servers or the FX80 supervisory controller as part of such a system.