Tenant Access - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Tenant Access allows the local system user or Active Directory service user to access all authorized features of the SCT UI. Tenant Access users can log on the SCT UI, but do not have log on privileges to the SMP UI.