Welcome - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Welcome to the System Configuration Tool (SCT) Help. This help file contains information on how to use the SCT user interface software. This section provides links to the major sections of the help file. It also provides an overview of SCT, its modes, and its access types.

Note: Throughout this help file, the term Site Management Portal (SMP) refers to the user interface of the online Metasys engines and servers as well as the offline SCT. For Facility Explorer (FX) users, the term SMP refers to the user interface of the online F4-SNC Supervisory Controller. The Metasys system uses the word Engine rather Supervisory Controller but these designations are interchangeable.