Factory Supplied SCT Summary Definition Templates - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Table 1 describes the pre-built SCT Summary Definition Templates. The templates include the definition name, default columns (in English only), and overview description indicating typical rows, key data, and other useful information that you can import into the SCT Summary Definition folder. You can use the SCT Summary Definition editor to rename and edit these definitions.

You can access a set of pre-built Summary Definitions through the License Portal. You can download the Summary Definitions when you download the SCT software, or as a separate download. To Download the Summary Definitions, complete the following steps:
  • Log on to the License Portal.
  • Click the Download icon for the System Configuration tool.
  • Select the SCT Summary Definitions check box, and then click Download.
  • Import the pre-built Summary Definition files into your site.

We designed the pre-built Summary Definitions to meet the needs of the users based on common tasks and functions. The Summary Definitions fit into the following main categories: Configuration, Diagnostics, and Monitoring (HVAC). The Site Administrators are the intended audience for the Device and Network Diagnostics definitions. Service Professionals will find the links to graphics and Key Point definitions in the Mechanical Equipment definitions especially useful.

Note: The SCT installer does not include the factory provided Summary Definitions Templates. You can download these templates from the License Portal, which you can then import into the SCT Summary Definitions folder. To import, right-click the SCT Summary Definitions folder and use the Import Definition selection to add the templates to a site's archive.
Table 1. Factory Supplied Default SCT Summary Definitions
Summary Definition Name Description / Use Case Default Column Headings Attribute ID Number
Engine Config and Diagnostic Tabs After you select Engine Devices in the All Items tree, all of the configurable attributes of the selected devices in the Configuration and Diagnostic tabs appear in the columns. Description 28
Firmware Version 44
Max message Buffer 848
Internode Comm Timer 845
Alarm Repository Size 32543
Alarm Snooze Time 32544
Event Action When Full 4296
Ack Forward Enable 64025
Audit Repository Size 32545
Audit Forwarding Threshold 32546
Audit Action When Full 32547
Audit Generate Alarm When Full 32548
Enabled Audit Level 32549
Power Sampling Interval 32550
Power Consecutive Samples 32551
JCI Exception Schedule 2573
ADS Repository 32558
ADS Connection Type 32559
ADS Priority Threshold 2586
ADS Delivery Time 32560
Network Tolerance 864
Engine Config BACnet After you select Engine Devices in the All Items tree, all of the configurable attributes of the selected devices in the BACnet tab appear in the columns. Description 28
User Name is BACnet 1092
Object Identifier 75
BACnet IP Port 1223
Process ID List 64010
Location 58
Restart Notifications Recipients 202
Time Sync Recipients 116
UTC Time Sync Recipients 206
Time Sync Interval 204
Align Intervals 193
Interval Offset 195
IEIEJ A List 755
IEIEJ A Period 756
Engine Email Tab After you select Engine Devices in the All Items tree, all of the configurable attributes of the selection devices in the Email tab appear in the columns. Description 28
SMTP Server Host 32537
SMTP Port 32538
Authentication Type 3814
SMTP Username 3815
POP Server Hostname 32540
POP Server Username 35239
From Email Address 32568
SSL Email Enabled 64590
SSL Email Ignoring Errors 64591
Engine Network Tab After you select Engine Devices in the All Items tree, all of the configurable attributes of the selection devices in the Network tab appear in the columns. IP Address 1135
IP Mask 1136
IP Router Address 1137
Obtain DNS Address 32533
DNS Server IP Addresses 32534
ADS Dialup - Connect Using 32575
ADS Dialup - ISP Username 64603
ADS Dialup - Enable DHCP 1138
ADS Dialup - IP Address 1135
ADS Dialup - Obtain DNS 32533
ADS Dialup - DNS Server IPs 32534
BACnet Routing - Mode 4307
BACnet Routing - Integrated Objects 4302
Engine SNMP Tab After you select Engine Devices in the All Items tree, all of the configurable attributes of the selection devices in the SNMP appear in the columns. Description 28
SNMP Enabled 32552
SNMP Trap Version 32622
SNMP Management Device 32553
SNMP Request Port 1180
Contact Person 32554
Public Community Name 32555
SNMP Trap Message Format 4188
Extension - Analog Alarm After you select Alarm Extensions from the Global Search results, all of the configurable attributes of the extension appear in the columns. Item Reference 32527
Description 28
Enabled 673
Event Enable 35
Report Delay 2294
High Alarm Limit 631
Low Alarm Limit 632
Single Setpoint Ref 109
Warning Ref 627
Cooling Setpoint Ref 1417
Heating Setpoint Ref 1418
Occupancy Ref 1419
Unoccupied State 1420
Differential 637
High Warning Offset 635
Low Warning Offset 636
Reference Delay Time 551
Alarm Ack Required 530
Alarm Priority 534
Warning Ack Req 520
Warning Priority 524
Normal Ack Required 525
Normal Priority 529
Alarm Message Text 536
Graphic 32581
Graphic Alias 32623
Object Identifier 75
User Name is BACnet 1092
Extension - Multistate Alarm After you select Alarm Extensions from the Global Search results, all of the configurable attributes of the extension appear in the columns. Item Reference 32527
Name 2390
Description 28
Enabled 673
Event Enable 35
Report Delay 2294
Normal State 646
Reference Delay Time 551
Command Reference 2394
Capture Changes 3400
Alarm Ack Required 530
Alarm Priority 534
Normal Ack Required 525
Normal Priority 529
Alarm Message Text 536
Alarm Values 7
Graphic 32581
Graphic Alia 32623
BACnet Object ID 1223
User Name is BACnet 1092
Extension - Totalization After you select Totalization Extensions from the Global Search results, all of the configurable attributes of the extension appear in the columns. Description 28
Object Type 79
Enabled 673
Item Reference 544
Timebase 2035
Totalize Limit 2037
Rollover 2038
Units 117
Display Precision 661
Extension - Trend After you select Trend Extensions from the Global Search results, all of the configurable attributes of the extension appear in the columns. Item Reference 544
Enabled 673
Start Time 142
Stop Time 143
Repository Enabled 2549
Transfer Setpoint 2550
Buffer Size 126
Client COV Increment 127
Sample Interval 2566
Stop When Full 144
Extension - Checker Advanced A selection of points from a device in the All Items tree of the result set of a Global Search can be viewed to check if Alarm, Trend, Totalization, Average, or Load extensions have been setup for the points. Point Description 28
Number of Extensions
Alarm Extensions
Quantity
Note: Child Item ::classid:156,172
65535
Trend Extension
Quantity
Note: Child Item ::classid:155
65535
Average Extension
Quantity
Note: Child Item ::classid:677
65535
Totalization Extension
Quantity
Note: Child Item ::classid:274
65535
Load Extension
Quantity
Note: Child Item ::classid:659
65535
Point Reference 544
Facility - Equipment Definitions After you select the Equipment Definitions Templates under the Definitions Folder, you can view all of the key attributes of the definitions to ensure consistency between all the definitions. Description 28
Object Type 79
Authorization Category 908
System Subtype Set 12169
System Subtype 12168
Facility - Equipment Serving After you select Equipment objects from the Equipment tab, you can view all of the serving relationships for a piece of equipment to ensure that the proper relationships have been created. Equipment Definition Used 6050
Equipment Served By 6049
Description 28
Authorization Category 908
Facility - Spaces to Equipment After you select Space objects from the Spaces tab, you can view all of the serving relationships for a Space to ensure that the proper relationships have been created. Space Type 3060
Equipment Serving Space 6049
Field Controller - MSTP After you select MSTP devices from the All Items tree, all of the configurable attributes of the devices appear in the columns. Item Reference 544
Description 28
MAC Address 2858
Disable Auto Alarming 1396
Enabled 673
Model Name 70
Firmware Version 44
Fixed Boot Version 884
Last Upload Date 64032
Last Upload Time 64301
Graphic 32581
Graphic Alias 32623
BACnet Object ID 75
User Name is BACnet 1092
Manual Time Sync Type 64030
Field Controller - N2 After you select N2 devices from the All Items tree, all of the configurable attributes of the devices appear in the columns. Item Reference 32527
Description 28
Controller Type 1357
Net N2 Address 806
Host Name 750
Disable Automatic Alarming 1396
Online Point Delay 758
Enabled 673
Graphic 32581
Graphic Alias 32623
Integration - LON After you select LON Integrations from the All Items tree or from a Global Search result set, all of the configurable attributes of the integration appear in the columns. Item Reference 32527
Description 28
Hardware - Neuron ID 32593
Resource File Language 32596
Domain ID 32594
Temporary Status Expire Time 3510
Status Launch Interval 3511
Integration - MSTP After you select MSTP Integrations from the All Items tree or from a Global Search result set, all of the configurable attributes of the integration appear in the columns. Item Reference 32527
Description 28
Hardware - Trunk Number 549
Hardware - Baud Rate Selection 2860
Hardware - Network Address 875
Object Type 79
Max Master 64
Max APDU Length 62
APDU Time out 11
APDU Segment Timeout 10
APDU Retries 73
Periodic Update 2192
Page Size 1181
Poll Delay 1163
Sync Time 32616
Sync Time Zone 64003
Discover All As Gen 1264
Requested Vendor ID 3675
Internode Comm Timer 845
Execution Priority 2197
Object ID 75
User Name is BACnet 1092
Integration - N2 After you select N2 Integrations from the All Items tree or from a Global Search result set, all of the configurable attributes of the integration appear in the columns. Item Reference 32527
Trunk Number 549
UDP Port 2558
Retries 1162
Poll Delay 1163
Message Timeout 1165
VAV Box Point Tester After you select VMA controllers from the All Items tree or from Global Search result set, common VAV mapped points appear in the columns based on point name matches. Description 28
ZN-T
ZN-H
ZNT-SP - NI
ZN-SP - AI
WC-ADJ
ZN-TOCC
HTG-O
SA-T
DA-T