Creating a New SCT Summary Definition - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Procedure

  1. Click Insert > SCT Summary Definition. The Create New SCT Summary Definition wizard appears.
  2. On the Identifier screen, enter a name for the SCT Summary Definition. Click Next.
  3. On the Configure screen, define the data of the SCT Summary Definition tab and the Configure tab.
    Note: One column is created by default when you create the definition and the user interface does not let you remove the last column. You must define a minimum of at least one column. You can add an unlimited number of rows or columns, but performance is resource-dependent and may be affected by large queries.
  4. Click Next. The Summary screen appears.
  5. Click Finish. The new SCT Summary Definition appears in the Configuration Data > SCT Summary Definitions folder.