Archive Database - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

An archive database holds the configuration information for the field devices and field points that make up a single site or multiple sites. The archive database contains information about controllers, input/output points, alarms, and device certificates. A single server can contain multiple SCT archive databases, Configuration Data, SCT Summary Definitions, and Controller Templates.