Menu Selection:
Figure 1. Manage Archive Wizard

Functions of the Manage Archive Wizard include the following:
- Upload Devices
- Upload CAF from Field Controllers (Release 6.0 or later)
- Download Devices
- Download Only Metasys UI Spaces and Equipment
- Download Supervisory Device Images (Code Download)
- Device Synchronization
- Device Upgrade and Migration
- Patch NxE55 Supervisory Devices
The Manage Archive Wizard uses the Action Queue (ActionQ) to initiate and monitor the load or backup/restore process. Access the Manage Archive Wizard by selecting Manage Archive from the Tools Menu. The Manage Archive Wizard collects information necessary to perform the load such as load type, controller names, and load time. Once you complete the wizard, the load commands are added to the ActionQ in the SCT. The ActionQ initiates and monitors the load.