Select
to modify a CAF in CCT and update the archive with these changes.Note: To use this feature, you must install both CCT and the SCT on the local computer. If
you connect to a remote installation of the SCT, you cannot use this feature.
After the CAF opens in CCT, the status Archive-Connected appears in the status bar. If you close the CAF or choose to disconnect from the archive, you invalidate the Archive-Connected state and, when saved, the CAF is not written back to the archive. You can use CCT to save a copy of the CAF and retain the Archive-Connected state.