You can commission N2 devices remotely from SCT using the Passthru mode. To perform Passthru, N2 configuration tools must reside on the computer with an SCT installed. You can launch Passthru applications from SCT or the online Metasys Site Management Portal UI. In addition, you can attach resource files, which are files created by N2 configuration tools, to field devices as extensions to assist with generating and mapping field points. See Table 1 for the file extension of the legacy tools supported by the engine.
|
Device/Controller Type |
Configuration Tool (M-Tool) |
File Name Expected during Import |
|---|---|---|
|
ASC |
HVAC PRO, LoaderUI |
PRN Note: When generating PRN files from the HVAC PRO, use the long
format.
|
|
VMA |
HVAC PRO |
PRN |
|
Vendor |
Vendor |
PRN |
|
XP |
XTM Configurator, LoaderUI |
HMC |
|
DX |
GX-9100 Tool, LoaderUI DX Commissioning Tool |
DMO |
|
MIG |
Metasys Integrator unit |
VCT |