Type |
Class Name |
||
---|---|---|---|
Controller |
Controller (N2 Controller) FEC Family BACnet Device |
LON Controller NCM |
Non-FEC BACnet Device VND Controller Wireless Receiver |
Device |
NCE25 (includes NIE29) NAE35 (includes NIE39) NAE45 (includes NIE49) |
NAE55 (includes NIE59) NIE55 NAE85 |
NIE89 CIE19 LCS85 |
Extension |
Analog Alarm Analog Load Analog Totalization |
Event Totalization JCI Averaging JCI Trend Log |
Multistate Alarm Resource File Multistate Alarm Runtime Totalization |
Folder |
Folder |
||
Integration |
BACnet Field Bus |
LON Trunk N1 Migration |
N2 Trunk VND Integration Wireless Supervisor |
NavList |
User View |
||
Object |
Async Delay Auto Shutdown Boolean Broadcast Management Comparison Conn DLLR DP Electric Demand Monitoring ENTH Enum Constant Flex Accumulator Global Data Graphic |
Interlock JCI AV JCI BV JCI Calendar JCI Event Enrollment JCI MV JCI Notification JCI Schedule Latch Math Multiple Command Mux Numeric Constant Optimal Start |
Pulse Meter Rate Limiter Release Object RH Sequencer Signal Select Summary Definition System Time Timer Trend Study Trigger Object XAML Graphic |
Point |
AI Mapper AO Mapper AV Mapper BACnet AI BACnet AO BACnet AV BACnet BI BACnet BO BACnet BV BACnet Grp BACnet MI BACnet MV BACnet Notification BI Mapper |
BO Mapper BV Mapper GIO LON AI LON AO LON MSI LON MSO MS/TP Pulse Counter MSV Mapper N1 AI N1 AO N1 BI N1 BO N1 Calendar N1 MSO N1 PC |
N1 PID Loop N1 Schedule N2 AI N2 AO N2 BI N2 BO N2 MSI N2 MSO N2 Pulse Counter VND AI VND AO VND BI VND BO Wireless Sensor |
Server |
ADS ODS |
||
Site |
Site |
Note: The devices NIE29, NIE39, NIE49, and NIE59 engines appear with the Class Name of
NCE25, NAE35, NAE45, or NAE55, respectively.