Re-indexing an Archive Database - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Using the Re-index feature improves SCT performance against large archive databases. The Re-index feature removes fragmentation from the archive database. Re-index works against any size archive and is especially recommended for sites containing more than 100 NxEs.

To re-index the archive database:

On the tools menu, select Database Re-index. A clock appears during the re-indexing process.