Re-index - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Menu Selection: Tools > Database > Re-index

Using the Re-index feature improves SCT performance against large archive databases. The Re-index feature removes fragmentation from the archive database. A clock appears during the re-indexing process.

Note: Re-index works against any size archive and is especially recommended for sites containing more than 100 NxEs.