Import Database - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Import Database option also imports the self-signed and trusted certificates for network engines only if they were part of the database export. If you want to include certificates, you need to specify the password that was entered when the database was exported. Without the password, you can import the database, but the certificate data is excluded.