System Preferences - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

System preferences apply to all users who log in to the site or device. System preferences affect the performance and operation of the system and require authorization to configure. A change to the audible alarm notification is an example of a system preference. Only the users defined in the Users Authorized to Edit System Preferences section are authorized to configure system preferences.

To synchronize system preferences within a site or to reuse the system preferences on another site, refer to the Configuring and Maintaining Preferences appendix of the ADS/ADX Commissioning Guide (LIT-1201645) , ODS Commissioning Guide (LIT-12011944) , or the NAE Commissioning Guide (LIT-1201519).