The Metasys Preferences dialog box is accessed through the Tools menu (Configure Preferences) and allows you to configure system and user preferences. Users authorized to edit system preferences can edit all preference fields using the Metasys Preferences dialog box. See Users Authorized to Edit System Preferences. Unauthorized users can edit only user preferences.
Some of the preferences defined in the Metasys Preferences dialog box also apply to the Metasys UI. The following table calls out the tabs with such preferences. See the specific tab section for details.
Click the tab name in the table for a description of the Metasys Preferences tabs. For more information on the modes of operation, see Modes.
| Tab |
SCT |
Applies to Metasys UI | Applies to SMP UI | Authorization Required |
|---|---|---|---|---|
|
X |
X |
|||
|
X |
X |
X |
X |
|
|
X |
X |
X |
X |
|
|
X |
X |