Graphic Settings Tab - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Graphic Settings tab allows you to configure the status colors, fan colors, and state colors that appear in standard and dynamic graphics, along with alarm flash settings. These settings apply to the Site Management Portal UI (online mode), SCT, and the Metasys UI. The status color settings may also be used by summaries or other views (Tailored Summaries, for example) to provide a consistent indication of an object’s status.

The following table describes the attributes of the Graphic Settings tab.

Table 1. Graphic Settings Tab

Field Names/Attribute

Description

Browse button

Accesses the Select a Color dialog box. The Select a Color dialog box allows you to select a custom color from three color palettes and to preview the color for the attribute.

Status Colors

Applies to value boxes, cells in Tailored Summaries, basic shapes (circle, triangle, and square), and the Room Status symbol used in floor plan-based graphics. See the Analog Alarm Extension for details on how these states are calculated.

Normal

Specifies the color used to indicate a status of Normal. The default color is white: RGB(255, 255, 255).

Out of Service

Specifies the color used to indicate a status of Out of Service. The default color is orange: RGB(255, 142, 25).

Overridden

Specifies the color used to indicate a status of Overridden. The default color is orange: RGB(255, 142, 25).

Trouble/Warning

Specifies the color used to indicate a status of Trouble, Low Warning, High Warning, or SAB Device Warning. The default color is yellow: RGB(255, 255, 0).

Offline

Specifies the color used to indicate a status of Offline. The default color is black: RGB(0, 0, 0).

Value Inaccessible

Specifies the color used to indicate a status of an inaccessible value (for example, communications failed). The default color is gray: RGB(190, 190, 190).

Alarm

Specifies the color used to indicate a status of High Alarm, Low Alarm, Alarm, or SAB Device Alarm. The default color is red: RGB(255, 0, 0).

Above Setpoint

Specifies the color used to indicate a status of Above Setpoint. The default color is pink: RGB(191, 0, 95).

Below Setpoint

Specifies the color used to indicate a status of Below Setpoint. The default color is blue: RGB(0, 0, 255).

Unoccupied

Specifies the color used to indicate an Unoccupied status. The default color is dark gray: RGB(150,150,150).

Fan Status

Allows you to customize the fan status color of the attribute that appears in system graphics. The Fan Status colors apply only to fans.

Stopped

Defines the background color used for a fan symbol when its bound object’s value indicates the fan is stopped.

Stopped is defined as State 0 (for binary/multistate objects) or as zero (for analog objects).

The default color is red: RGB(255, 0, 0).

Running

Defines the background color used for a fan symbol when its bound object’s value indicates the fan is running.

Running is defined as State 1+ (for binary/multistate objects) or as non-zero (for analog objects).

The default color is green: RGB(0, 153, 51).

Default State Colors

Allows you to customize the default state color of the attribute that appears in system graphics. The Default State Colors apply to basic shapes (circle, triangle, square) that are bound to a binary/multistate object. These default state colors can be changed for each shape after it is added to a graphic.

State 0

Specifies the color used for the State 0 setting of a dynamic graphic symbol. The default color is white: RGB(255, 255, 255).

State 1

Specifies the color used for the State 1 setting of a dynamic graphic symbol. The default color is green: RGB(0, 153, 51).

State 2

Specifies the color used for the State 2 setting of a dynamic graphic symbol. The default color is red: RGB(255, 0, 0).

State 3

Specifies the color used for the State 3 setting of a dynamic graphic symbol. The default color is blue: RGB(0, 0, 255).

All Other States

Specifies the color used for the All Other States setting of a dynamic graphic symbol. The default color is light gray: RGB(204, 204, 204).

Simple Symbol Flash Settings

Allows you to customize simple UGT shapes (such as circles and squares) to flash when their bound object is in alarm.

Flash Type

Defines the type of flashing applied to basic shape symbols:

  • Disabled (No Flashing)
  • State Color/Alarm Color (Flashes between the State Color and Alarm Color)
  • State Color/Alternate Color (Flashes between the State Color and Alternate Color)

The default value is 0: Disabled (No Flashing).

Alternate Flash Color

Defines the color used when flashing between the current color and an alternate flash color. The default color is white: RGB(255, 255, 255).

Flash Rate

Defines the flash rate for graphics symbol flashing. The range is from 100 to 1,000 ms. The default value is 250 ms.