Preferences - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The Metasys system provides customized preferences for the user interface. The preferences allow you to configure how the user interface behaves, including its sounds and colors, startup views, alarm priorities, and the ability to add links to external applications that can be accessed from within the UI.

Some of the preferences defined in the Metasys Preferences dialog box also apply to the Metasys UI. The Metasys Preferences Dialog Box section calls out such preferences.