Exporting a Certificate - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

To export a certificate for a network engine in an archive database:

Procedure

  1. Open the archive database.
  2. On the Tools menu, select Certificate Management. The Certificate Management screen appears.
  3. Click the Devices tab. A table of devices with certificates appears. Select the device whose certificate you want to export.
    Figure 1. Exporting a Certificate

  4. Click Export Certificate(s). The Export Certificates dialog box appears.
    Figure 2. Export Certificate(s) - Select Folder Screen

  5. Click Export Certificate(s). The certificate file is exported to the selected folder location. For example, if the name of the NAE is NAE-1, the certificate file would be called NAE-1.pem.