Print - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Procedure

  1. Select the navigation tree or display panel you wish to print.
    Note: You must select either the navigation tree or a display panel to enable Print. If you selected a display panel, the entire contents of the visible display panel prints out. If you selected the navigation tree, all visible parts of the tree print out (even parts of the tree that you need to scroll to view). Collapsed parts of the tree (not visible in the tree) do not print. You cannot print the contents of the Alarms Window.
  2. Select Page Setup from the Item menu if you wish to change the paper, orientation, or margin size. Click OK when done.
  3. Select Print Preview from the Item menu to see what the printout looks like. Click Print or click OK.
  4. On the Item menu, select Print.
    Note: If the panel you selected is not printable, Print is disabled.